AXIS#.MOTOR.TYPE
Description
AXIS#.MOTOR.TYPE sets the motor type and the torque
Torque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist control algorithm for the motor. The following table provides the motor types:
| AXIS#.MOTOR.TYPE | Motor and Control Type |
|---|---|
| 0 | Rotary surface permanent magnet motor |
| 2 | Induction motor with V/Hz open loop |
| 4 | Induction motor with closed loop |
| 6 | Rotary interior permanent magnet motor |
| 10 | Rotary Surface Permanent Magnet (SPM) motor with sensorless control |
-
-
This parameter is automatically configured for Kollmorgen motors when AXIS#.MOTOR.AUTOSET=1 and motor memory version is 0.3 or greater. This parameter can be modified while AXIS#.MOTOR.AUTOSET = 1 if its AXIS#.MOTOR.DISAUTOSET index = 1.
-
-
ECCN 3A255 imposes special limitations on operating speed for induction motors. See ECCN 3A225 Limitations for Induction Motors.
Each motor type has a set of parameters that must be configured either through automatically setting them to values in motor memory (when AXIS#.MOTOR.AUTOSET = 1) or through manual user settings. The list of required parameters are reported by AXIS#.SETUPREQLIST which updates when the motor type changes. When any of the required parameters are not configured, the drive reports : Faults and Warning Messages (Drive motor parameters setup incomplete) on the axis.
The following parameters are required for rotary surface permanent magnet motors (AXIS#.MOTOR.TYPE = 0 or 10):
The following parameters are required for linear SPM motors (AXIS#.MOTOR.TYPE = 1):
- AXIS#.MOTOR.ICONT
- AXIS#.MOTOR.IPEAK
- AXIS#.MOTOR.LDLL
- AXIS#.MOTOR.LQLL
- AXIS#.MOTOR.PITCH
- AXIS#.MOTOR.POLES
The following parameters are required for induction motors with open loop V/f control (AXIS#.MOTOR.TYPE = 2):
The following parameters are required for induction motors with closed loop control (AXIS#.MOTOR.TYPE = 4):
- AXIS#.MOTOR.ICONT
- AXIS#.MOTOR.IMID
- AXIS#.MOTOR.IMTR
- AXIS#.MOTOR.IPEAK
- AXIS#.MOTOR.LDLL
- AXIS#.MOTOR.LQLL
- AXIS#.MOTOR.POLES
The following parameters are required for rotary interior permanent magnet motors (AXIS#.MOTOR.TYPE = 6):
- AXIS#.MOTOR.ICONT
- AXIS#.MOTOR.IDMAX
- AXIS#.MOTOR.IPEAK
- AXIS#.MOTOR.KE
- AXIS#.MOTOR.LDLL
- AXIS#.MOTOR.LISAT
- AXIS#.MOTOR.LQLL
- AXIS#.MOTOR.PHSADVK1
- AXIS#.MOTOR.PHSADVK2
- AXIS#.MOTOR.POLES
- AXIS#.MOTOR.VOLTMAX
Context
For more information see Motor.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 | |
| Feature change | 02-01-01-000 | Added type 1 for linear SPM. |
| Feature change | 02-06-01-000 | Added type 10 for rotary SPM with sensorless control. |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0, 1, 2, 4, 6, 10 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
See Also |
N/A |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.MOTOR.TYPE | 0x500B | 0x4 | USINT | - | - | RW | False |
| AXIS2.MOTOR.TYPE | 0x510B | 0x4 | USINT | - | - | RW | False |